7/1/2016 7:33 AM | |
Posts: 2 Rating: (0) |
Dear Mr Ayman Elotaify Can u elaborate on how to make the adapter as u have mentioned above.. |
7/1/2016 8:00 AM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (708) |
6AV6671-8XD00-0AX0 - Product Details - Industry Mall - Siemens ... |
2/22/2018 5:35 PM | |
Posts: 1 Rating: (0) |
Yes Please elaborate. My M5 PG is still a few weeks out and my boss doesnt want to spend the $600 for the adapter |
2/22/2018 6:43 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (708) |
Hello, if it is for 6AV6671-8XD00-0AX0 is 9 pin male and 9 pin female 1:1 you can buy one 9 pin male and one 9 pin female and 9 wire and connect 1 to 1 , 2 to 2 and so on |
5/9/2018 9:35 AM | |
Posts: 10 Rating: (0) |
Having problem with factory resetting MP277 Touch panel,. First we try with Ethernet but no factory reset option will appear in prosave os_update section, or the mac address of panel not on the back of the screen. Then we try with PPI multi master that's works for us, but after successfully Reset procedure we again got the same problem the panel stuck on boot manu. please give some more suggestion to way out. thanks in advance AttachmentMP277 Problem.pdf (659 Downloads) |
5/16/2018 3:49 PM | |
Joined: 5/28/2008 Last visit: 9/30/2024 Posts: 4515 Rating: (839) |
Hello, It seems that you selected the wrong cable to update OS. First please download attached excel sheet in the following entry: Which connector cables are available for connecting to SIMATIC Panels? after revising for your panel, you can only update OS using RS232-PPI cable or right angel adapter. Hope this helps. |
Ayman Elotaify |
|
Follow us on