5/25/2023 1:37 PM | |
Joined: 1/21/2013 Last visit: 8/4/2024 Posts: 3044 Rating:
|
Hi SMsib, To start a program on your device, you can use the StartProgram system function. The scripting engine of WinCC Unified does not have the same functionality as the browser. However, you should be aware that StartProgram cannot start a program with a user interface. Kind regards |
5/26/2023 12:05 PM | |
Joined: 8/12/2019 Last visit: 7/19/2024 Posts: 19 Rating:
|
Hello, Thank you for your answers. I try to run programs even without a user interface (both exe and bat) but without success. I tried to follow step by step the example of rdoliveira in the third suggested link ( How to run the script so that it is tied to a button click event in the HMI? - 299797 - Industry Support Siemens ) but without success: is it necessary to configure the browser or the project in some way? |
Follow us on