4/4/2012 6:41 PM | |
Joined: 9/24/2010 Last visit: 4/21/2024 Posts: 118 Rating: (10) |
Let me try more. Thank you so much
|
Mechatronic Center |
|
4/6/2012 8:58 AM | |
Joined: 8/31/2010 Last visit: 11/6/2024 Posts: 1523 Rating: (229) |
Hello Tranhieu0983, Enclosed is the Address in STEP 7 Classic and STEP 7 - TIA Portal v11. STEP 7 Classic: The red highlighted area in image "01_STEP 7 Classic" thas the addresses. STEP 7 - TIA Portal v11: The red highlighted area in image "02_STEP 7 - TIA Portal v11 - 02" has the addresses. In S7-1200 for having addresses in DB you have to choose Block Access as Standard, as shown in Image "02_STEP 7 - TIA Portal v11 - 01" AttachmentDB.ZIP (2446 Downloads) |
Like it? Rate it! |
|
This contribution was helpful to5 thankful Users |
3/16/2017 12:44 PM | |
Posts: 1 Rating: (0) |
Bit = "DBName".Tag.x0 Byte ="DBName".Tag.B0 This Tag is not working as I want to use bit of "int" type register |
3/16/2017 1:11 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi Swandra, this works only with the datatypes Byte, word and double-word. see the FAQ: Bewerten How in STEP 7 (TIA Portal) do you access the unstructured data types bit-by-bit, byte-by-byte or word-by-word and symbolically?hope this helps, regards, |
FCK WAR! |
|
3/16/2017 1:29 PM | |
Joined: 12/9/2016 Last visit: 1/13/2022 Posts: 243 Rating: (127) |
it works the same also for INT DINT SINT USINT UDINT data types.
|
If you find my contribution helpful please RATE it :)) |
|
This contribution was helpful to1 thankful Users |
Follow us on