11/8/2016 10:27 AM | |
Posts: 4 Rating:
|
Hi Cristoph, I have a problem like that; i have a real PLC 1214 DC/DC/rly and v13 tia portal sp1 upd 9 and win cc advanced sp1 upd 9. ı wrote a plc program and a panel program but i havent got a real panel. when i want to click run time buton, i looked it is grey and passive. how can i see that the panel program runs or doesnt? i select hmi panel ktp 700 basic. And i have to say that i can run the program in simulator without any problem. I wanna work only runtime. Please help me. Best regards Murat ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 11/8/2016 10:40:02 AMNew subject after splitting |
|
11/10/2016 11:50 AM | |
Joined: 5/12/2006 Last visit: 6/26/2024 Posts: 22278 Rating:
|
Hi, and which access path is configured in the HMI Connection in TIA? Christoph |
11/10/2016 11:02 PM | |
Posts: 4 Rating:
|
you can see in the photo my access path. when i click the runtime button it makes error |
Follow us on