5/17/2022 9:17 AM | |
Joined: 11/4/2011 Last visit: 9/20/2024 Posts: 233 Rating: (26) |
Hi there, how the parameter can be written can be seen here in the manual, see column "Access" and also column "W" (for when the change gets effective): https://support.industry.siemens.com/cs/de/en/view/109773400/127258120587 Legend with the meaning of these parameters can be found here: https://support.industry.siemens.com/cs/de/en/view/109773400/127630039691 In your case, as you have mentioned you have a PTO axis, this means that you can change the parameter via instruction MC_WriteParam, when the TO is disabled (MC_Power.Status=FALSE). Change is made effective when axis gets enabled again. Information on MC_WriteParam can be found here: https://support.industry.siemens.com/cs/de/en/view/109773400/126823329803 Regards, |
Follow us on