12/10/2013 10:40 PM | |
Posts: 8 Rating: (0) |
I opened a service request and attached the log files. I'll post back when I get a responce. |
12/11/2013 3:22 PM | |
Joined: 3/20/2013 Last visit: 4/3/2024 Posts: 676 Rating: (44) |
let me know what they tell you. you checked already all FW versions and they are uptodate? There is no other AP the clients can connect to? (your signal strength sounds OK) The AP has the whole time connection to the LAN and you have not configured "Force roaming on LAN interface down" or sth. like that? |
Best Regards, |
|
12/11/2013 3:58 PM | |
Posts: 8 Rating: (0) |
I checked all of that except the FW version. I'll look into that now. I have the iPCF enabled now and that's when my log fills up. When it's disabled everything works like a champ. There's only one client and one AP invloved. I'm not sure why my customer wants this enabled. |
12/11/2013 4:05 PM | |
Joined: 3/20/2013 Last visit: 4/3/2024 Posts: 676 Rating: (44) |
One last thing: you have chosen a higher actualisation time for the PNIO devices behind the iWLAN clients? Depending on the further traffic on your network / WLAN ... the iPCF makes your communication deterministic (time slots for each iWLAN Client). I guess you know that and think with the little load on your network there should be no problem? |
Best Regards, |
|
12/11/2013 6:53 PM | |
Posts: 8 Rating: (0) |
Ok, it looks like I resolved my issue. I have everything enabled that my customer requires including iPCF. Apparently there was some interference on the 2.4GHz band. I changed my frequency band to 5GHz and my client and AP Associated with one another (one time). I have yet to seethem becomeDisassociated. Always something simple. |
This contribution was helpful to2 thankful Users |
Follow us on