9/28/2021 11:56 AM | |
Joined: 4/10/2021 Last visit: 3/21/2024 Posts: 70 Rating: (6) |
Hi I have written codes in PCS 7 v9.0 (+WinCC 7.4) and want to test it using S7-PLCSIM. I followed instructions found in the thread: https://support.industry.siemens.com/tf/ww/en/posts/pcs7-simulate-wincc-with-plcsim/164434 but firstly when I opened PLCSIM , the mode is in STOP mode and I can not change it??? after that when I download the hardware, codes, connection some error appear as the attached file,,, I can not find the error causes?? and finally when I open a CFC in CFC editor , how can I start monitoring it (after downloading to the simulator)??? Please help me solve above problems Thanks so much AttachmentCompile and Download Objects.txt (171 Downloads) |
Follow us on