1/31/2023 8:16 AM | |
Joined: 5/17/2013 Last visit: 4/30/2024 Posts: 14 Rating: (1) |
After installing TIA V18 in the Win 11 pro 2022H2 operating system, the emulator PLCSIM V18 cannot be started. The error message says .NET is not installed ( can't power on instance ). Now I have resolved this exception message, please refer to the following steps for specific methods... 1. Go to the Microsoft website to download the software https://dotnet.microsoft.com/en-us/download/dotnet < .Net Download 2. Download 6 software and Installation 1) dotnet-runtime-5.0.14-win-x86.exe 2) dotnet-runtime-5.0.14-win-x64.exe 3) dotnet-runtime-6.0.9-win-x64.exe 4) aspnetcore-runtime-5.0.14-win-x86.exe 5) aspnetcore-runtime-5.0.14-win-x64.exe 6) aspnetcore-runtime-6.0.8-win-x64.exe 3. Remove the new version before installation, if it is already installed dotnet-runtime 6.0.9 => removed dotnet-runtime 5.0.17 => removed 4. After the installation is complete, Restart the computer 5. Enjoy
|
Last edited by: Masabubu at: 02/02/2023 03:10:02Last edited by: Masabubu at: 02/02/2023 03:12:14Last edited by: Masabubu at: 02/02/2023 03:14:13Last edited by: Masabubu at: 02/02/2023 03:17:48Last edited by: Masabubu at: 02/06/2023 02:33:27Last edited by: Masabubu at: 02/06/2023 02:34:05お疲れ様です, 毎度お世話になります |
|
This contribution was helpful to4 thankful Users |
8/17/2023 4:19 AM | |
Joined: 3/30/2020 Last visit: 10/14/2024 Posts: 4867 Rating: (995)
|
Thank you for sharing your insights. Please could you tell us which is the exact version of PLCSIM you are using at the moment. Now (2023/08/23) the latest is V18 SP1 Update 1. You can get updates from [Updates for STEP 7 V18, S7-PLCSIM V18 and WinCC V18]. Also mention which Windows version. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on