2/13/2013 4:00 PM | |
Posts: 836 Rating: (100) |
Hi, when the port is there it should work though? You could could use a null modem calbe to establish a conenction to another computer with rs232 port. There are several infos on the internet about null modem communication, like this. Iam not sure how it works for windows but should be possible anyway. |
2/13/2013 4:43 PM | |
Joined: 4/23/2010 Last visit: 11/14/2024 Posts: 8092 Rating: (878) |
Hi, Thanks for your interest & reply. So could you explaine lit bit further, as how to proceed further after connecting two PCs thru the ports as explained in link? |
2/13/2013 5:59 PM | |
Joined: 4/23/2010 Last visit: 11/14/2024 Posts: 8092 Rating: (878) |
Please see the attached file. Courtesy : Mr. Ekalavya - Attachmenthow_to_check_the_comport[1].pdf (931 Downloads) |
This contribution was helpful to1 thankful Users |
2/13/2013 6:10 PM | |
Joined: 3/21/2006 Last visit: 11/1/2024 Posts: 10229 Rating: (1181) |
Why that procedure is not valid for Windows7? Sorry, I can not catch it? |
2/13/2013 7:18 PM | |
Joined: 3/21/2006 Last visit: 11/1/2024 Posts: 10229 Rating: (1181) |
Aaa, I didn't noticed that. Because I asked one griend he suggested me thatputtysoftware like an alternative together withWinSCP |
This contribution was helpful to1 thankful Users |
2/14/2013 5:00 AM | |
Joined: 4/23/2010 Last visit: 11/14/2024 Posts: 8092 Rating: (878) |
Thank you for the interest & reply.Is this for HyperTerminal communication? |
2/14/2013 7:19 AM | |
Joined: 3/21/2006 Last visit: 11/1/2024 Posts: 10229 Rating: (1181) |
As I understood yes. What do you have doubts about COM port there? best regards, Hristo Mihalev
|
Follow us on