5/11/2021 4:27 PM | |
Joined: 7/7/2010 Last visit: 5/13/2024 Posts: 14710 Rating: (2363) |
I recommend updating the PLC firmware to the latest available before deciding which TIA Portal version you need. Since you can only purchase licenses from Siemens for the "current" version (today, that's V16), it would make sense to start with the version with the most device support and provided features.
|
science guy |
|
5/11/2021 6:02 PM | ||
Joined: 1/26/2014 Last visit: 5/9/2024 Posts: 164 Rating: (0) |
I tried with TIA V15.1 But it gives error that configuration was made with an earlier version. So its mean i can try with TIA V14?? |
|
5/11/2021 6:09 PM | |
Joined: 1/26/2014 Last visit: 5/9/2024 Posts: 164 Rating: (0) |
I also tried with TIA V13 SP2. it gives again error. Snapshot is attached. I will try now with V14 |
5/17/2021 1:59 PM | |
Joined: 3/11/2019 Last visit: 5/14/2024 Posts: 1410 Rating: (255) |
Hi jabbi_king, there are some dependencies for uploading a project. In most cases you will need the version of TIA the cpu was configured with initally. There is also an FAQ for that. If the CPU was configured with >=V14, you can see the project version of the cpu in the online & diagnostics page. (Offline screenshot attached, after connection online to the cpu, you can see the project version) What options are available in STEP 7 (TIA Portal) for uploading when the project version in the CPU no longer matches the version on your PG/PC?
regards sancruz |
Feedback appreciated, please rate |
|
5/17/2021 3:36 PM | |
Joined: 6/19/2019 Last visit: 5/10/2024 Posts: 694 Rating: (72) |
V14 SP1 |
8/13/2021 3:02 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello jabbi_king regarding to the firmware V2.1 for S7-1500 CPUs you need TIA Portal V14 SP1 or higher. See also the FAQ for your support if you want to upload the program from the CPU in the PG: In STEP 7 (TIA Portal), how do you load the "Program Blocks" with the PLC tags and PLC data types from the CPU into the programming device? With best regards |