11/28/2015 12:31 PM | |
Posts: 53 Rating: (0) |
Hi I use TIA v13 create FC. I want to use bit memory from byte memory in the FC.How to work on it. Thanks. |
11/28/2015 1:33 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (819) |
Hello, f.ex. if your Tag_1 is %MB0, last bit is: "Tag_1".%X7 mean M0.7. |
With best regards... |
|
11/28/2015 5:36 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating: (705) |
Hello abbot, In addition to our friend Duris_I, This is for V11 but take a look below the FAQ |
11/29/2015 7:29 AM | |
Posts: 53 Rating: (0) |
I found this. |
11/29/2015 8:05 AM | |
Posts: 53 Rating: (0) |
Not work. |
11/29/2015 8:08 AM | |
Posts: 1529 Rating: (202) |
What error are you getting when you mouse over the coil? My test works fine. (V13 sp1, S71200) |
11/29/2015 8:54 AM | |
Posts: 53 Rating: (0) |
Please send demo program to me. Thanks. |
Follow us on