5/22/2012 12:59 PM | |
Posts: 18 Rating: (0) |
hi! i am new to this type of programming. Pls guide right from the 1st step. So that i can perform data transfer bet two siemens PLC using BSEND & BRCV Adios
|
5/22/2012 1:20 PM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hello Adios, How do you program communication blocks FB12 "BSEND" and FB13 "BRCV" for data exchange in the S7 program of an S7-300 CPU? Step by Step with Example..... Also Very good Document, CPU-CPU communication with SIMATIC controllers (compendium) |
Last edited by: Ammy at: 5/22/2012 1:23 PMCPU-CPU communication with SIMATIC controllers (compendium) link added Ammy |
|
5/22/2012 3:02 PM | |
Posts: 18 Rating: (0) |
hello, i am using CPU315 & ethernet model - CP 343-1 TCP.
|
5/22/2012 3:15 PM | |
Posts: 691 Rating: (37) |
Have you configured Communication Partner in Netpro and downloaded it to the CPUs? |
5/23/2012 7:13 AM | |
Posts: 18 Rating: (0) |
hello, the mentioned got resolved when i selected station as (unspecified). I am using the following hardware. 1) CPU 315-2DP - 2NOS 2) CP343-1 Advanced. - 2Nos Now if i use CPU 315 & CP 343-1TCP (which client is using) . the previously mentioned issue persist? Why is it so? Adios... AttachmentBSEND_BRECV.zip (378 Downloads) |
5/23/2012 7:52 AM | |
Posts: 1064 Rating: (72) |
Can you post a screen shot of your netpro setup ,it doesn't sound like you have them configured in netpro |
5/23/2012 8:18 AM | |
Posts: 3093 Rating: (323)
|
|
Last edited by: Kaulquappe at: 5/23/2012 8:26 AMdeleted - I was on the wrong way Last edited by: Kaulquappe at: 5/23/2012 8:24 AM |
|
Follow us on