2/29/2024 11:18 AM | |
Joined: 2/29/2016 Last visit: 5/15/2024 Posts: 2 Rating: (0) |
I have to use one main program for engraving letters from A to Z and numbers from zero to nine. I need to select any one alphabet randomly and any one number randomly to create any word maybe 12-15 letters ( including repeated alphabets as i desire e.g A LL E P E ) . I have separate subprograms created for each of these engraving letters and numbers. In all 36 subprograms are available for engraving each letters or numbers in CMA folder . How can i define them as variable in GUD and then use them in my mpf file to be executed for engraving. Currently i am calling each required subprogram in my mpf file & using them as required . I want to use them in customised screen . Kindly guide.
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 03/01/2024 10:14:00New subject after splitting |
|
Follow us on