11/12/2018 7:56 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (379)
|
Hi community, there is an instruction created by the Leuphana University how to connect the IOT2000 to the MindSphere using the MindConnect Lib. It includes a step-by-step procedure of how to build the MindConnect Library inside the IOT2000, how to onboard, send timevalues series and send a file to MindSphere. Many thanks to the University for posting this! Best regards! AttachmentDocumentation_SimaticIOT2000_MindsphereSiemens.pdf (1462 Downloads) |
Last edited by: bergmanu at: 11/12/2018 7:56:24 AMNot working for IOT2050 support anymore from March 1st, 2024. |
|
12/31/2018 7:59 AM | |
Posts: 2 Rating: (0) |
Hi, I faced the same issue before, my IoT2040 image version is v2.1.3, you may try the solutions as follow: Step 1, Check the dependencies of libmc.so with command:
example:
Check if the libmc.so is correctly dependent to the path of libssl, libcrypto which you have built. if the solution not work,continue step 2. Step 2, Before you execution the binary file of you program, configure system environment LD_LIBRARY_PATH to the library path of libmc.so libcrypto.so libssl.so libcurl.so
if the solution not work, continue step 3. Step 3, Rebuild all library, if the solution not work, continue step 4. Step 4, Update your IoT2040 system to newest official version and rebuild all. Best Regards |
This contribution was helpful to3 thankful Users |
Follow us on