3/14/2016 9:14 AM | |
Posts: 21 Rating: (0) |
i am new in plc programming. can anyone explain me how to use the feedback of a level transmitter that connected ti AI card. how to use that to on a motor when low and off the motor when high. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/15/2016 10:05:34 AMNew subject after splitting |
|
3/14/2016 9:23 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Level sensor feed back is DI or AI? Confirm. If analog, is it 0-10 V or 0-20 mA or 4-20 mA? Which AI module you use? |
3/14/2016 11:21 AM | |
Posts: 21 Rating: (0) |
6ES7 331-1KF02-0AB0 its an analog input module |
3/14/2016 11:42 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
You have not specified the type of your float sensor i.e. is it current or voltage base. Please read this link which shall help you. |
3/14/2016 11:54 AM | |
Posts: 21 Rating: (0) |
current based 4-20mA |
3/14/2016 12:23 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Read this post. |
Follow us on