7/2/2013 3:34 PM | |
Posts: 6 Rating: (0) |
Thanks hdhosseini, along with 150 motors i also need RS 485 communication board . Is it available in s7 300. |
7/2/2013 6:25 PM | |
Joined: 1/28/2009 Last visit: 5/19/2024 Posts: 6840 Rating: (1359) |
Hello, personally I don't recommend using a personally developed TON to be used instead of standard functions.You can check it here in STL for S7 300/400.You can develop a same idea.Memory required for DB to keep data of my function FB1 is around "140 bytes".It is atrade off between reliability and cost reduction. Best regards Hamid Hosseini |
7/18/2013 8:13 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Follow-up question splitted to is it possible to find which input i received first in the CPU? Best regards O_Moderator |
Follow us on