6/27/2024 5:56 AM | |
Joined: 8/3/2009 Last visit: 7/2/2024 Posts: 13174 Rating: (1676)
|
Hello StalinCode The Trends in a Trend Control are a collection of trends. Each Trend has own properties. To get access to the different trends in Runtime with a Script you can set the trend Index before to switch between the trends. If you want to dynamize the Trends in Runtime with different Tags you can use a script. Look at this example: https://support.industry.siemens.com/cs/de/en/view/10259719 Its an old WinCC V7 FAQ but It will work (for example the VBS) also for WinCC Prof. It shows you how to change the Tagname that is configured on a Trend. If you then change an Index or prefix in the Name via script you can change between the Motors. Another way would be to work with screen windows an a Tag prefix. Then the Tag change could be used dynamically. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on