9/9/2016 10:00 AM | |
Joined: 4/4/2015 Last visit: 12/4/2020 Posts: 12 Rating: (0) |
Thank you very much, it is very helpfull. |
This contribution was helpful to1 thankful Users |
9/10/2016 3:26 PM | |
Joined: 3/30/2011 Last visit: 4/25/2024 Posts: 733 Rating: (255) |
Hello, segment 3 activate output A12.4 80ms after both input E4.1 AND E4.0 goes high. Segment 2 and 4 is for direct access to I/O. Normally I/O are updated at beginning/end of scan cycle. With L PY and T PY I/O are updated during the cycle. About german/engish mnemonics translation in this manual (appendix A) you can see the complete instruction list in both languages. Hope this helps, for other doubts please ask. Have a nice week-end!! |
★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ |
|
This contribution was helpful to1 thankful Users |
9/18/2016 2:42 PM | |
Joined: 3/30/2011 Last visit: 4/25/2024 Posts: 733 Rating: (255) |
Hello kusha02,
better way to say thank you is to use "To thank" and "Rate" button (this say also to other user that this thread contain useful info)
in my previous post there is a link to the SIEMENS manual "From Step5 to Step7", in appendix A (Address and instruction list, starting from page 131 of pdf document) there is a complete list of command in both languages. this is the link https://support.industry.siemens.com/cs/ww/en/view/1118413 Why you cant find?????
i dont use pg2000 but on internet you can access complete documentation with instruction to change language....... attacched image pg2000 language window from documentation......
|
Last edited by: mindware at: 9/18/2016 2:48:22 PM★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ |
|
This contribution was helpful to1 thankful Users |
Follow us on