1/9/2018 6:36 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating:
|
Hello Ixspm8888, I'm not sure if I understand your last question. I think
looks alright.
I guess at least one of should work, too. Can't test it atm. Might depend on the runtime. If you want to use a system function in the script, add it on the right side in the "Function list" window, add the parameters, click on the space in the code where you need it and then click on "Apply". It's added in the correct syntax, too. - "What is the relationship between object and object type in WinCC (TIA Portal)?" Greetings, H.J.
|
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
Follow us on