11/5/2013 8:25 AM | |
Joined: 4/22/2010 Last visit: 2/26/2025 Posts: 5697 Rating:
|
Hello, I'm not sure what you are trying to do there, but perhaps this helps. How do you proceed when peripheral device errors are detected by the S7-1200? Regards, Marcjan |
Problem solved? |
|
11/5/2013 9:09 AM | |
Joined: 3/10/2013 Last visit: 2/5/2025 Posts: 11 Rating:
|
Yes i create project like this but does not work. What i need ; i trie use OB82 to check if cabel on Profinet be disconnect from PLC ( port PN X1 i have 1215DC/DC/DC) to HMI (KTP400 mono PN) and the connection be broken ( like wire demage ) . Next when this problem be on the PLC must show error LED. This is my screen
Attachmentscreen.zip (567 Downloads) |
Follow us on