12/18/2020 12:34 PM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Please see the attached screenshots. I need to program a PLC, a drive and a flex panel to control a cutting machine. I am starting with the HW configuration and I have added the components and named them and assigned IP addresses. But where do I set / see the drive specifications in TIA portel so I can ensure the programming match the actual drive? AttachmentED1 programmering b.zip (148 Downloads) |
12/18/2020 12:45 PM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating: (3006)
|
check the folder "Ungrouped Devices" |
This contribution was helpful to1 thankful Users |
12/18/2020 1:43 PM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating: (3006)
|
in the details if you select the drive |
This contribution was helpful to1 thankful Users |
12/21/2020 7:28 AM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating: (3006)
|
Hi, open the details view of the device (Device view) |
Follow us on