2/28/2022 12:43 PM | |
Joined: 4/1/2015 Last visit: 10/11/2023 Posts: 9 Rating:
|
Hello bergmanu, how will the "FS:02" devices be rolled out? Do they get a new order number or can we randomly get a FS:02 shipped when we order? Is this roll out already in progress? Also what does PG stand for? Best regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/01/2022 09:16:37New subject after splitting |
|
3/1/2022 7:55 AM | |
Joined: 4/28/2015 Last visit: 11/28/2023 Posts: 3287 Rating:
|
Hi, yes, if you place an order today, you will receive a FS:02 device. Depends on which 1.x.x image your stick is based. EDIT: This is not true! Basic FS:02 and Advanced FS:04 cannot run Example Image V1.1.1! They require from V1.2.1 I think it would make sense to update the software to the Example Image V1.2.x, as it runs a newer kernel (5.10) and Debian 11. "Old" devices can still use Example Image V1.2.x, therefore the firmware needs to be updated. Best regards! |
Last edited by: bergmanu at: 03/04/2022 15:16:22Correction of Image compatibility |
|
3/1/2022 9:59 AM | |
Joined: 4/28/2015 Last visit: 11/28/2023 Posts: 3287 Rating:
|
Hi, yes, same is valid for IOT2050 Advanced from V1.1.1. EDIT:This is not true! Basic FS:02 and Advanced FS:04 cannot run Example Image V1.1.1! They require from V1.2.1 There is no deprecation warning, we update the downloads here and inform in this thread. You can set this thread as Favorit and receive notifications for it. Best regards! |
Last edited by: bergmanu at: 03/04/2022 15:16:58Correction of image compatibility |
|
This contribution was helpful to
1 thankful Users |
Follow us on