1/7/2019 1:09 PM | |
Joined: 1/17/2018 Last visit: 9/10/2024 Posts: 24 Rating: (2) |
Dear Wüstenrauber, how would a topology look like if we used the integrated PN port for both Master and Slave communication? Do we need to use Scalance switches to connect many TCP slaves to the S7-400? Only controller redundancy is needed, field devices are not redundant but they must connect to the redundant controller. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 1/8/2019 10:44:03 AMNew subject after splitting |
|
Follow us on