1/25/2013 12:48 PM | |
Posts: 4 Rating: (0) |
Hello I have a request for assistance. The HSC (TIA Portal "S7-1200 controller 1212C AC / DC / RLY") should make counter revolutions per minute. Reference is 1000 impuzov / minute is 200Hz. As the show would be on the touch panel KT 400th I am done according to the instructions is attached below .. Please if you can help me to end applications.. I'm a beginner. Regards Attachmenthsc.zip (815 Downloads) |
Last edited by: tdi at: 1/26/2013 12:30 PMLast edited by: tdi at: 1/25/2013 12:49 PM |
|
10/5/2015 1:03 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
New question published by Fsoares01 is split to a separate thread with the subject Simulate pulses in the HSC 1 input in the PLCSIM v13?. Best regards |
Follow us on