1/28/2013 9:58 AM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (135) |
Hallo, please find the FAQ (link) in the internet and perhaps it could be support for you: http://support.automation.siemens.com/WW/view/de/41995947 Consider also the accuracy by the REAL numbers. Generally speaking, it holds that REAL numbers are specified and calculated with an accuracy of 6 decimal places. With the calculations you should also note that this accuracy holds for every single step of the calculation. http://support.automation.siemens.com/WW/view/de/14844391 Mit freundlichem Gruß |
Follow us on