3/7/2024 7:46 PM | |
Joined: 12/15/2023 Last visit: 5/10/2024 Posts: 18 Rating: (0) |
Good morning I am developing a project on s7-1200 and I activate the web server of the automaton to create a page on the web. I have looked at the videos on the net and programmed everything well as well as the html code but I cannot get it change the variables on the automaton, yet with the web page, we can force them. Does anyone have an html code for a simple engine start with 2 buttons? or if you had this problem? thank you could you make me an html file with 2 push buttons to control a motor, thank you email gerard.raynal0130@orange.fr I am desperate. Thank you
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 03/08/2024 14:05:18New subject after splitting and text formatting optimized |
|
3/8/2024 2:09 PM | |
Joined: 8/21/2014 Last visit: 5/16/2024 Posts: 960 Rating: (13) |
Closed cause question posted twice. The second thread with the subject cpuc1215c dc/dc/rl is published within the conference SIMATIC S7-1200 Best regards, |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to1 thankful Users |
Follow us on