4/30/2024 11:14 AM | |
Joined: 6/18/2020 Last visit: 5/2/2024 Posts: 9 Rating:
|
Hello to everyone. I have pcs7 step7 v5.5_sp4+hf9 and i want to update the HW/config in order to install the 6ES7155-5AA01-0AB0 in my project. Is it possible? will i install the card via gsd or HW update? in my project i already have the 6ES7155-5AA00-0AB0 can i use this? in the manual say: Engineering with
• STEP 7 TIA Portal configurable/integrated
as of version
V14 or higher with HSP 0223 / integrated with
V15 or higher
• STEP 7 configurable/integrated as of version
GSDML V2.32
• PROFINET as of GSD version/GSD revision
V2.3 / Thanks in advance. |
Last edited by: polyzos at: 04/30/2024 11:17:49 |
|
4/30/2024 11:24 AM | |
Joined: 3/11/2019 Last visit: 7/26/2024 Posts: 1528 Rating:
|
Hi, as stated in the delivery release for 6ES7155-5AA01-0AB0: Sales and delivery release of revised version of the standard IM 155-5 PN ST interface module for ET 200MPCompatibility:The revised module with the Article No.6ES7155-5AA01-0AB0is spare parts compatible with the predecessor module Article No.6ES7155-5AA00-0AB0which it replaces. When replacing the -5AA00- with a -5AA01- (spare parts case), the previous configuration can be retained without the need for any changes ----------------------------- So yes, it should be possible to use th "old" product number in hw-config. Otherwise you can install the latest GSDML file for ET200MP system, but there can potentially be issues with GSDML file version with older versions of STETP 7 or PCS 7. regards sancruz |
Feedback appreciated, please rate |
|
4/30/2024 11:37 AM | |
Joined: 6/18/2020 Last visit: 5/2/2024 Posts: 9 Rating:
|
thank you very much |
This contribution was helpful to
1 thankful Users |
Follow us on