3/5/2022 1:05 PM | |
Joined: 3/5/2022 Last visit: 4/23/2022 Posts: 3 Rating:
|
Hello everybody, i need some information for PXC001 and modbus TCP. I read on release note that now is possibile to integrate also modbus TCP, but how is programmed in CFC? Just write point in this sintax? M=11(3.0.4104.0.0[UINT32])/T=192.168.1.1 (as written in release note) Without any "com" block? ......................... It's possible to make the PXC001 "slave"? In my case i have to communicate via modbus TCP with a PLC, but the PLC is "master" Last question: the same port is for both modbus TCP and Bacnet? Thanks to all! ......................................................... |
3/5/2022 10:01 PM | |
Joined: 10/17/2007 Last visit: 7/14/2024 Posts: 4008 Rating:
|
Hello Friend, make sure you not enter the wrong forum. What system you use?
|
If you like my comments please |
|
Follow us on