11/25/2019 11:03 PM | |
Posts: 3 Rating: (0) |
Thanks pal, I found the application you are talking about. I believe it will be suitable for me. As I understand when selecting a communication telegram between the drive and the PLC during commissioning it is automatically inserted in the S1500 Motion Control FB of the technology object and I don't need to deal any more with it.I need just to specify for which axis I am using the FB. Am I right? I was confused because I found one application that used custom FB and the telegram had to be specified in the function blog.(FB file attached). Please correct me if I am wrong. Attachment109741575_MC_PreServo_and_MC_PostServo_v10_en.pdf (640 Downloads) |
Follow us on