1/29/2010 5:04 PM | |
Posts: 4 Rating: (0) |
Hi I am doing the first example of the c-script course you attached and I am getting really strange output. Please somebodycheck theattached files (one with the script and second with the output) and tell me if unsigned long and unsigned int have value ranges 0 to 4294967295 why in my case the output is 2147483648 for both. Thank you in advanse! Best regards, Momchil Attachmentattach.zip (40 Downloads) |
Last edited by: O_Moderator at: 2/1/2010 8:43 AMnew subject after splitting from /tf/WW/en/Posts/38447#top Last edited by: kid42day at: 1/29/2010 5:11 PM |
|
1/29/2010 8:52 PM | |
Posts: 27 Rating: (2) |
Unlessand until youare looking for very WinCC specific commands (Which can be sorted by above Attachemnts. Rest can Be sorted by Google. Type VBS/C which ever you want prior to the logical query of your requirment. e.g. If you want to create a folder on your computer using VBS Type vbs make directory in google search bar. You can click on"Create folder in vbscript" link from the searchresult. Answer is: Sub CreateFolder( strPath ) On Error Resume Next If strPath <> "" Then 'Fixes endless recursion in some instances when at lowest directory If Not objFSO.FolderExists( objFSO.GetParentFolderName(strPath) ) then Call CreateFolder( objFSO.GetParentFolderName(strPath) ) objFSO.CreateFolder( strPath ) End If End Sub Regards, KD... |
1/30/2010 2:48 PM | |
Posts: 4 Rating: (0) |
KD... I don't want to create folder with VBS... |
2/2/2010 3:47 AM | |
Joined: 4/23/2007 Last visit: 5/20/2024 Posts: 58 Rating: (3) |
Is there a link where I can download SP1 and HF4? If so, I can test it. Regards, Wave |
"There is no spoon." |
|
2/2/2010 9:38 AM | |
Posts: 4 Rating: (0) |
Thismust be thelinks: |
Follow us on