4/5/2024 3:58 PM | |
Joined: 5/28/2008 Last visit: 8/6/2024 Posts: 4515 Rating:
|
Hello, First you have to convert your project to any comfort panel. Then you should use tool "Data2Unified Add-in" from this link: Data2Unified Add-in The generated file should be used by WinCC Unified. So you should have WinCC Unified to work with Unified Panels.. And for more details, have a look here: Guide for switching from Comfort Panels to Unified Comfort Panels and from WinCC Runtime Advanced to WinCC Unified PC Runtime |
Ayman Elotaify |
|
4/9/2024 5:23 AM | |
Joined: 8/31/2010 Last visit: 8/7/2024 Posts: 1519 Rating:
|
You can refer more details here - Data2Unified Add-in (Current Version - V3.2.0.0) Using this version "Conversion of SIMATIC HMI Basic Panels to SIMATIC HMI Unified Basic Panels" is supported. Also, the above link has documentation and video on how to use the Data2Unified Add-in. Hope this helps. |
Last edited by: Jen_Moderator at: 04/09/2024 11:36:04Link optimized. Like it? Rate it! |
|
Follow us on