7/3/2023 10:24 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983) |
Winccflex do not support this panel. |
7/3/2023 10:28 AM | |
Joined: 5/6/2022 Last visit: 5/9/2024 Posts: 419 Rating: (82) |
Hi dindyk, I have been checking the panel reference, and if you look at the technical data you can see that this panel is not configurable in WinCC flexible. It is configurable in the TIA Portal since version V11 SP2. I share the technical data where you can find this information: "6AV6647-0AK11-3AX0: SIMATIC HMI KTP400 Basic Color PN" I hope this information can help you. Best regards! |
If this Information really helps, you could use the Rate function |
|
7/3/2023 10:36 AM | |
Joined: 7/1/2020 Last visit: 4/23/2024 Posts: 9 Rating: (0) |
OK Thanks you very much for the information and help. Have a nice day |
Follow us on