Industry Online Support
Technical Forum
7/3/2011 4:00 PM | |
Posts: 118 Rating: (4) |
Hi All Anybody tested on these DP Slave diagnostics behind Y-Link. Now I am in need of using the same. need to read the Node failured behind Y-Link and message to SCADA. I have DP/DP Coupler and ASi Master connected behind the Y- Link and need to display the node failure of all ASi Slaves. can anyone help? attached is the hardware config Splitted from System Diagnostics of ET200S Profibus Slaves in Y-Link. AttachmentDoc1.pdf (298 Downloads) |
Last edited by: O_Moderator at: 7/4/2011 12:33 PMnew subject after splitting |
|
7/4/2011 12:46 PM | |
Joined: 10/3/2008 Last visit: 4/6/2024 Posts: 954 Rating: (123)
|
Hi, I attach 2 pictures about the diagnosis. It's shown whether the slaves behind the y-link are okay or not okay. It's the same in a h-system. I don't know a difference by using SFC13. Have a look at the manual of the h-system. Wüstenräuber AttachmentSystemdiagnose.zip (331 Downloads) |
Follow us on