3/16/2011 10:19 AM | |
Posts: 7 Rating: (0) |
I have Win7 Ultimate 32 Rus and Starter 4.2 and 4.1.5.5 Installation reports that can not start S7EINSTX.DLL for both versions. I tried to install without joining in domain and with joining in domain as user with user domain rights but local administrator. When installing with rights of the domain administrator - no problems. Readme studiously read. All rights as local and domain user "Siemens TIA Engineer" and "Network configuration operators" is present.There is this problem for all users and W7 computers in domain in company. Splitted from Starter v4.2 on Windows7 problem. |
Last edited by: O_Moderator at: 3/17/2011 8:42 AMnew subject after splitting Last edited by: AndVinni at: 3/16/2011 10:26 AMLast edited by: AndVinni at: 3/16/2011 10:24 AM |
|
3/16/2011 12:39 PM | |
Joined: 5/12/2006 Last visit: 7/16/2024 Posts: 22316 Rating: (2998)
|
Hello, Starter V4.1.5.5.is not released for Windows 7! Which STEP7 is installed on the system? Regards Christoph |
3/21/2011 3:23 PM | |
Posts: 7 Rating: (0) |
Splitted from Starter v4.2 on Windows7 problem.
|
Last edited by: AndVinni at: 3/21/2011 3:26 PM |
|
3/21/2011 3:25 PM | |
Posts: 7 Rating: (0) |
Starter V4.1.5.5.is not released for Windows 7! Which STEP7 is installed on the system? I know. I have reported this for the best understanding the problem. |
Follow us on