1/13/2015 7:52 AM | |
Posts: 8946 Rating: (999) |
Dear Marko, hard to advice you without knowing what exactly you need to do. A small "brainstorm": 1.) WinAC RTX is very fast. Evenlarger programs run with few ms. µs is not possible, I don't think so. I do not find any instruction-scantime list, but I am quite shure RTX is fast as a 15xx CPU at least. What PC? Some IPC or Panel-PC is a good selection. 2.) S7-1518 Even ifSiemens like to tell us something different, the 15xx CPU are still "stuck in its infancy". I have some friends and customers that try the 15xx System. Without exception they are disappointed There are (a lot) of problems with the Firmware, the TIA Portal bring still the problems that we all know already. If you like to use 15xx System, be sure you have enough time and nerves.... 3.) Simotion... Do you take a look to Bosch-Rexroth Indradrive Inverters? They are easy to use and the communication to PLC is a joy, compared with Siemens - "Toolboxes". |
This contribution was helpful to2 thankful Users |
1/17/2015 4:59 PM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (153) |
:) The other manufactures not so big and shinny are in advantage,also if they did a comprehensive work. Have you ever heard about this company: https://www.rexcontrols.com/rexlib-blockset They have their PLCopen motion blocks. |
Follow us on