5/7/2009 9:25 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Dear AhmedFM, Perhaps this link might help: http://support.automation.siemens.com/WW/view/en/19449428 Or this link: http://support.automation.siemens.com/WW/view/en/6518822 Best regards, Wizard |
5/7/2009 3:31 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating:
|
Hello Ahmed, You could be use also DP/DP Coupler if both CPU are master. Is this system old (exist only local CPU with ET200 slaves) and you need to add another CPU. Then you should to decide. This CPU will be master or slave. If this will connect like profibus slave, follow Wizard's advices. In the other way, if this CPU will master (with own profibus slaves) then use DP/DP coupler. How to use DP/DP coupler look at manual. DP/DP Coupler Hope this will helps. Best regards Hristo MIhalev |
Follow us on