12/19/2008 9:11 AM | |
Joined: 2/5/2007 Last visit: 9/9/2023 Posts: 101 Rating: (10) |
Hi! I've developed a FB to handle pressure sensors which has profibus interface. When I developed the FB I connected three sensors to a 315-2 DP. Everything is working on my test system. But when I implemented the FB to my customers system I sometimes, say 1 of 5, get I/O access error when triggering the FB. I'm attaching the diagnose buffer. I don't think it says more than I just explained. Can it be something with the bus? Bus parameters, timeout? I know they have some OBT's and four operator panels. AttachmentIO access error.pdf (176 Downloads) |
12/19/2008 10:22 AM | |
Joined: 2/5/2007 Last visit: 9/9/2023 Posts: 101 Rating: (10) |
Ok. So you say. I thought 4 panels wouldn't be any problem. The same customer has one system with 11 panels without any I/O eccess error I attach a schematic drawing of the network. AttachmentProfibus network.pdf (155 Downloads) |
12/23/2008 12:15 AM | |
Joined: 10/7/2005 Last visit: 5/8/2024 Posts: 3004 Rating: (1046) |
Dear Dande74 if you are really using OBT's your firstproblem is that you are only allowed to connect ONE device to its RS485 port! Please check the Simatic Net Profibus networks manual for more on this (link: http://support.automation.siemens.com/WW/view/en/1971286). If you need to keep the topology as is, youshouldreplace the OBT's with OLM's (note that OBT's use plastic fiber so the OLM version needs tobe a "P"one). Other things to check are correct termination of each RS485 copper segment(Terminator must beON at the Start and End of each RS485 Segment). I hope this helps and make sure to have a merry X-Mas. |
Cheers |
|
12/29/2008 9:06 AM | |
Joined: 2/5/2007 Last visit: 9/9/2023 Posts: 101 Rating: (10) |
Thanks for the suggestion. I'll try this aswell. Will come back with a report as soon as I have tested. |
Follow us on