10/6/2023 12:53 PM | |
Joined: 8/3/2009 Last visit: 9/18/2024 Posts: 13728 Rating: (1728)
|
Hello JoshJDMFG there are different possibilities for using Recipe Screens without the Recipe Control Table. There are a set of systemfunctions for creating, loading, tranfering ´, saving Datasets and so on that you can use without using the recipe control. You can also use the recipe control only for selectint the datasets -> disable the table and the buttons and just use the drop down lists and use the tags for selected dataset for loading the datasets in the IO Fields with systemfunction. You can set also in the settings of the recipe how it should act .. online or offline Examples for Recepe screens are here: https://support.industry.siemens.com/cs/ww/en/view/109739999 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on