6/11/2012 9:16 AM | |||||||||||||||||||
Joined: 10/3/2010 Last visit: 7/31/2024 Posts: 1560 Rating:
|
Check this: WinCC Information System -> Working with WinCC -> Creating Process Pictures -> Working with Objects -> Working with Objects in the Object Palette -> Working with Smart Objects -> I/O Field -> How to define the output format for the "String" data type Formatting codes - "String" data type The allowed length of a character string is defined by the number of formatting codes used (exception "*").
|
||||||||||||||||||
B r g d s , |
|||||||||||||||||||
This contribution was helpful to
3 thankful Users |
6/11/2012 9:54 AM | |
Posts: 1776 Rating:
|
Fine answer. Rated with stars |
This contribution was helpful to
2 thankful Users |
Follow us on