Industry Online Support
Technical Forum
11/15/2010 9:19 PM | |
Posts: 16 Rating: (0) |
I have some doubts about memory in S7-300 and S7-400, if anyone can help me I will give five stars: [schnippschnapp] If I use "Save project to memory card"I generate a compressed file ,if the energy down the compressed file is not uncompressed by plc, for restarting,in otherwords,whetherI want the backup that could be used for restarting I would need Copy Ram to Rom, However If I do that I will erase the card? Splitted from Is there a way of saving the symbolic in S7-300 and S7-400?. |
Last edited by: O_Moderator at: 11/17/2010 9:51 AMnew subject after splitting Last edited by: Clodoaldopuc at: 11/15/2010 11:33 PMLast edited by: Clodoaldopuc at: 11/15/2010 9:24 PM |
|
11/16/2010 9:50 AM | |
Joined: 4/24/2006 Last visit: 12/20/2024 Posts: 8786 Rating: (1172) |
Dear Clodoaldopuc, Let try to give you some information. [schnippschnapp] Perhaps the following links, might help to answer the question: /tf/WW/en/Posts/26251 SIMATIC Programming with STEP 7 V5.5 SIMATIC S7-300 CPU 31xC and CPU 31x Technical specifications SIMATIC S7-400 S7-400 Automation System, CPU Specifications Best regards, Wizard |
Last edited by: O_Moderator at: 11/17/2010 9:59 AM |
|
Follow us on