5/12/2010 10:04 AM | |
Joined: 6/3/2009 Last visit: 9/14/2022 Posts: 118 Rating: (2) |
Hi Hristo, did you try anything regarding this issue or not? regards |
5/14/2010 9:08 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello, Sorry for the delay. Better later then never. Anyway, so just finished with settings and everything works properly. I'll write again some important point: 1. PG/PC Interface - PLCSIM (TCP/IP). 2. IP address in PC and CPU must be the same. 3. Put in command line - net stop s7oiehsx and click OK. (remove problem with port 102). 4. Download program to PLCSIM and put in run CPU. 5. Start nettoplcsim and click connect. You will receive message PLCSIM connected, listening for client. 6. Start Window Viewer. (if settings in SMC and Maker are correct, even without correct seetings) you should receive Client: IP address and port number 7. Probably most important thing is (just looked for some reason to disconnect or block connection between PLCSIM and INTOUCH) always you must have ethernet cable connected to netwrok adapter of PC. If you don't have message local area connection is connected, or disconnect this tool nettoplcsim failing. Look at attachment. There has some screenshots. If you want I could send also Step7 and Intouch test projects. AttachmentMy Pictures.zip (671 Downloads) |
5/14/2010 2:41 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Take my test projects. If your hardware configuration isn't compatible.(I don't think but...). About SQL server I don't know. But basically also don't think there have problem. For me the problem is in sequences. It's not possible to be other. I tried even in virtual mashine works fine. PLCSIM5.4 SP3 NetToPLCSim | Get NetToPLCSim (downloaded from there)Step7 5.4 SP5 Intouch 10.1 (DEMO version). Before I had been installed 10.0 (not demo) also works. AttachmentSIM.zip (526 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on