3/29/2011 4:39 AM | |
Posts: 9 Rating:
|
Dear engineer |
3/29/2011 4:54 AM | |
Joined: 10/7/2005 Last visit: 10/4/2023 Posts: 2991 Rating:
|
Hello Moong I'm afraid to say that that is NOT possible. Whatyou can do to link "non-redundant"DP slaves on a "non-redundant"Profibus line tothe redundant Profibus of an S7-400H system is touse the so called "Y-Link" and below are a few links with more info on this: How is the Y link structured? Bus links DP/PA coupler, DP/PA link and Y link manual I hope this helps |
Cheers |
|
3/29/2011 7:14 AM | |
Posts: 9 Rating:
|
i under stand. if i can redundant configuration. i use Y-link. ok very thank you. |
This contribution was helpful to
1 thankful Users |
Follow us on