Industry Online Support
Technical Forum
10/5/2010 9:19 PM | |
Posts: 34 Rating: (0) |
Dear NSPK thnks for ur rply 2nd Q is that i want to make a redundant connection for wincc7.0 with S7-400H system. plz note that i dont want to use CP1613 or any other special hardware for redundant connection.I want to do it by using common LAN card installed in my PC and doing something in wincc7.0. Regards PLC engineer Splitted from I want to make 2nd ET's module as a redundant for 1st ET. |
Last edited by: O_Moderator at: 10/6/2010 1:38 PMnew subject after splitting |
|
10/6/2010 1:39 PM | |
Joined: 4/24/2009 Last visit: 8/2/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already discussed in the following thread Is there any function like change connection in winccflexible?. Best regards O_Moderator |
Follow us on