Industry Online Support
Technical Forum
3/5/2010 12:05 PM | |
Joined: 6/3/2009 Last visit: 9/14/2022 Posts: 118 Rating:
|
Hi to all, I have a problem. I wanted to conect PLC and 2 RIOs. Because the distance between then is >800m, I wanted to conect them through FO. I put in RIOs IM 153-2 FO, but then I saw that the max distance for them is 300m (with some special cables). Now I have to choose another solution to my problem. I saw these PROFIBUS OLM G11 and G12. But now I'm not sure, which IM should I have, to make this conection. Maybe my picture in attach says more. Or should I choose another PLC and RIOs? Can I use the PROFIBUS interface from the PLC after to conect to a switch (Profibus/ethernet)? Or the best solution is to choose IMs with ethernet interface and through switches (ethernet to FO) to go through long distances? Thanks in advance AttachmentPLC with 2xRIO.pdf (86 Downloads) |
Last edited by: O_Moderator at: 3/9/2010 8:29 AMnew subject after splitting from /tf/WW/en/Posts/14625#top |
|
Follow us on