Industry Online Support
Technical Forum
6/15/2012 2:35 PM | |
Posts: 14 Rating:
|
I would like to file gsd. Mp277 8 "touch [6AV6 643-0CB01-1AX1]. Thank you. |
6/15/2012 3:22 PM | |
Joined: 9/27/2006 Last visit: 6/8/2023 Posts: 12037 Rating:
|
Hello msarapong; Why? What exactly do you want to do with this gsd file? Make the MP277 a slave to a 3rd-party DP-master? Use the Direct Keys configuration on Profibus-DP? In Siemens's world, an operator panel does not operate as a slave on Profibus-DP; it is a Master Class 2, and has all the rights of any other master on the bus. So the above questions would mark the only reasons you would need the gsd file ofan operator panel;. Look at the following FAQ for more answers, and further links: Which GSD files are there for the Profibus DP operator panels? Hope this helps, Daniel Chartier |
6/17/2012 8:21 AM | |
Joined: 4/24/2009 Last visit: 2/23/2023 Posts: 2685 Rating:
|
Thread closed, because question is already published in the following thread The gsd file. mp277 8" touch Best regards O_Moderator |
Follow us on