7/9/2019 2:51 AM | |
Joined: 4/28/2015 Last visit: 8/9/2019 Posts: 10 Rating: (0) |
Hi Davide, Unfortunately, I still got the error for c-project: i586-poky-linux-gcc: error: CreateProcess: No such file or directory or for c++ project: i586-poky-linux-g++: error: CreateProcess: No such file or directory The paths are adapted as described from you by replacing 6.2.0 with 7.3.0. I can also look at the paths at the tree as shown in screenhot no.7 of your attachment (zip). Where is my error? Should I change in addition some other settings -e.g., C/C++ Enviroment variables such as PATH or POKY_HOME? ------------------------------------------------------------------------------------------ |
Last edited by: lbomboes at: 07/09/2019 02:53:22Last edited by: lbomboes at: 07/09/2019 03:08:56Last edited by: lbomboes at: 07/09/2019 03:09:15Last edited by: Jen_Moderator at: 07/10/2019 08:52:31New subject after splitting |
|
7/9/2019 7:00 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, Running 7-Zip as admin solved the issue, as explained in this thread. Kind regards! |
7/9/2019 7:38 PM | |
Joined: 4/28/2015 Last visit: 8/9/2019 Posts: 10 Rating: (0) |
Missing administrator credentials of 7zip was the issue. Now every works fine. Thank you for help! Lars |
Follow us on