1/20/2009 11:46 PM | |
Posts: 2661 Rating: (279)
|
Hi, Can you provide more information how this was done? I was not aware that the standard AddFEM (6DL3100-8AC) can be upgraded to AddFEM SoE (6DL3100-8AC03) or AddFEM PoCo (6DL3100-8AC02). For both these FEF's the configuration is done via HW config and CFC channel drivers (see attachment). Additional hardware neededper order numbers above. Regards AttachmentAddFEM.pdf (293 Downloads) |
1/21/2009 8:18 PM | |
Posts: 2661 Rating: (279)
|
Look in the Module Information (HW Config-Online) for the order number. See attachment.
AttachmentAddFEM_ModuleInfo.pdf (245 Downloads) |
Follow us on