3/30/2009 1:50 PM | |
Posts: 61 Rating: (0) |
Dear Expert, As per the enclosed PDF file, will this configuration work? If yes, How? Thanks AttachmentIE_PB_LINK.pdf (276 Downloads) |
3/30/2009 4:18 PM | |
Posts: 61 Rating: (0) |
Thank you very much . I got your point and we will go for Ethernet CP's. Sir pls help me in below query I wants to connect fixed printer ( having serial port) to the moving S7 300 PLC. How can this possible ( which hardware / software required). I have suggested one example in attached file ( PLC+ Serial CP+ Serial to IE converetor+Access point ( WLAN)<----> Client module( WLAN)+IE to serial converetor( same one)+Printer). will it work? AttachmentVisio-Drawing1.pdf (111 Downloads) |
Follow us on