7/11/2024 5:04 PM | |
Joined: 4/28/2015 Last visit: 7/13/2024 Posts: 2 Rating:
|
Hello, I am a trainer and I would like to present the programming of S7-1200 (TIA v19) PLCs as closely as possible to the IEC 61131-3 standard. I'm using this document [STEP 7 Standards compliance according to IEC 61131-3 (3rd Edition)] dated April 2015. I don't know if there is a more recent one? In this document, page 23, table 25. AttachmentIEC_61131_compliance_en_US.pdf (3 Downloads) |
Last edited by: Wit_Moderator at: 07/12/2024 12:54:27File attached from link |
|
7/12/2024 8:15 AM | |
Joined: 4/28/2015 Last visit: 7/13/2024 Posts: 2 Rating:
|
An other example The standard contains the mentions of CONCAT_DATE_TOD and CONCAT_DATE_LTOD. In the help : T_COMBINE: Combine times (S7-1200, S7-1500) « Note Use of T_COMBINE in SCL programs When you drag the instruction "T_COMBINE" from the "Instructions" task card to the SCL programming window, the internal instruction CONCAT_DATE_TOD or CONCAT_DATE_LTOD is displayed there. » Standard and TIA STEP 7 use different names. |
7/12/2024 5:57 PM | |
Joined: 7/7/2010 Last visit: 7/12/2024 Posts: 14948 Rating:
|
Be sure and enable IEC check for every created block in that case. It's a property for OBs/FCs/FBs (or attribute depending on your thoughts). Default is unchecked.
|
science guy |
|
Follow us on