2/13/2024 12:50 PM | |
Joined: 8/12/2021 Last visit: 7/3/2024 Posts: 316 Rating: (29) |
Hi! There is a manual available for this library. In the documentation, it is indicated (page 10) that for an S7-400, for example, there can be up to a maximum of 8 connections. These blocks consume CPU scan time. To consult more information, there is an email indicated: function.blocks.industry@siemens.com. Maybe they can secure you the number for an S7-1500. |
Last edited by: The Helping Hand at: 02/13/2024 14:02:39Text formatting optimized If this Information really helps, you could use the Rate function |
|
Follow us on